Part Number: LMK03328
Dear all,
Would you mind if we ask about Soft pin Programming Mode?
Our customer ask 3 questions like below.
1.In the case of Soft pin programing mode, Which of following GPIO2's and GPIO3's setting is correct at start up?
(1)VIH=1.4V~ (2)VIM=0.9V (3)VIL=~0.4V (4)No connection
2.The following description is given in Datasheet p.32 10.3.3.2 Soft Pin Programming Mode(HW_SW_CTRL=0).
http://www.ti.com/lit/ds/snas668d/snas668d.pdf
"The GPIO inputs[3:2] are sampled and latched at power-on reset (POR), and select one of 6 EEPROM pages which are custom-programmable. When GPIO[3:2] are left floating, EEPROM is not used and the hardware register default settings are loaded. Table 10, Table 11, Table 12, Table 13, and Table 14 show the predefined EEPROM configurations according to the GPIO[3:2] pin settings."
2-1.Is it correct that "hardware resister default settings" is Table 15,16(Default ROM Contents)?
2-2. Is it correct that Table10~14’s contents is the stored value at time of shipment and loaded setting when latched in the Soft pin Programming mode?
it would be great if you could let me know your thoughts on the following questions.
Best regards,
Y.Ottey