Other Parts Discussed in Thread: SN74AUC245
Hi,
I would like to interface two chips, Where VDDIO = 1.8V. Due to the negative noise margin issue I need to use a bidirectional buffer or level translator with better Voh, Vol. (Like Voh is more or equal to than 1.6V and Vol lesser or equal to 0.2V) . Pls suggest the suitable bidirectional auto detection translator or buffer with above requirement, Or is there any way to suppress this negative noise margin pls give advice on this.
Awaiting for the reply,
Thanks,
Vignesh