This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: GPIO2 and GPIO3 setting

Guru 19785 points
Part Number: LMK03328


Hi Team,

I found a typo. Could you please correct the table in the next datasheet update ?

In the following table, GPIO2 is listed as "Z" which means floating (open).

GPIO2, GPIO3 pins are 3-level pin, however, user cannot leave it floating (open). Instead, user would need  to apply VIM=0.9V.

Best Regards,

Kawai

  • Hi Kawai-san,

    I will not consider this a typo, we simply used a common engineering language to express the status of a 3-state logic pin: High, Low, or Hi-Z.

    I agree that maybe a more consistent expression here is use VIM instead of Z to represent the pin status when it is not 0 or 1.

    Thank you for your suggestion, we may modify it in the next revision.

  • Hi Noel-san,

    Thanks for the comment.

    It would be helpful if this could be modified to prevent confusion.

    Best Regards,

    Kawai