Part Number: LMX2595
Other Parts Discussed in Thread: , LMK61E2, LMK61PD0A2, LMX2594, USB2ANYWe recently purchased the LMX2595 EVM. When measuring the phase noise with a Keysight E5052B signal source analyzer, we noticed this board is very sensitive to the vibration of the table.
When we place the board on a stable table, the integral from 100Hz to 10MHz is less than 100fs. But if I connect the board to the E5052B directly, the instrument has a fan on it and the vibration is passed to LMX2595EVM, and the integral becomes 300-500fs or even worse. Put it back on the stable table, and tap with a pen, I can see the low-frequency noise goes up a lot. I want to know if this is a problem of the chip or the board, maybe some capacitor or inductor? Can you point to me which capacitor/inductor should be replaced to what to overcome this problem? Thanks