Part Number: LMK04610
Other Parts Discussed in Thread: LMX2581, LMX2572, LMX2582
Tool/software: WEBENCH® Design Tools
Dear TI,
I'm unable to model phase noise, jitter, or spurs for the LMK04610 with any of your simulation tools? For example, Webench returns a message along the lines that "Simulation is not yet enabled for this part." When will I be able to simulate the LMK04610?
I'm using the LMK04610 to create a 10MHz clock reference for your LMX2581 and a 200MHz sample clock with less than 100fs RMS jitter. I need a better idea of what frequency should be used for the LMK04610's reference input and what frequency should be used for the VCXO.
Any interim suggestions?
Thank you,
Jeff