Hi,
I have designed a tone generator using LMX2594. But, the phase noise performance of the tone generator is not matching the datasheet performance.
For example: For a 3.5GHz carrier at an output power of 2dBm, the phase noise performance is given below
Frequency Offset | Phase Noise(dBc/Hz) |
1kHz | -98.34 |
10kHz | -102.83 |
100kHz | -105.34 |
1MHz | -113.61 |
But, the datasheet performance(Page No. 12 in the LMX2594 datasheet) is given below
Frequency Offset | Phase Noise(dBc/Hz) |
1kHz | -106.8 |
10kHz | -117 |
100kHz | -119.7 |
1MHz | -130.6 |
What might be the reason for the degradation in the phase noise performance?
Regards,
Karthik