Part Number: TPL5111EVM
Other Parts Discussed in Thread: TPS61029, TPL5111
Hi Support,
Tested the DC/DC boost EVK.
Changed R2 to 1.5M ohm for VOUT to 4.3V.
The VOUT without load and it is working : 4.3V
After added the Load 100mA, the VOUT drop a bit to 4.12V.
Added 200mA loading, the VOUT become failed and no output voltage.
Because the datasheet TPS61029 don’t have the Vin VS I out chart reading.
I also do not know what happened, could you advise?
Thanks.