Part Number: BQ32002
Hi,
We want to measure the pin7 IRQ output of the RTC chip, configured as a clock output of 1HZ or 512HZ. Register 22 is configured by default to 0 and output 512HZ. When we configure the 1HZ output, register 22 is set to 0x1 and the setting is unsuccessful. Register 7 is already configured as 0xc0. Why is it that the setting of 1HZ is unsuccessful, and there are other places that need to be modified?