This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00105: 1PPS signal interfacing

Part Number: LMK00105

Hi Team,

We have a requirement to fanout 1PPS signal into two (one FPGA and one clock synchronizer) destinations, both destinations are at 1.8V logic. So we can set the Vddo at 1.8V. But the challenging point here is, we can't assure the voltage level of 1PPS input, it may be 1.8V or 3.3V. In this scenario, how we can set Vdd (Supply for operating core and input buffer) ? Also please help to fix the biasing for the same.

Best regards,

Shibili