Other Parts Discussed in Thread: CDCLVC1102, LMK04828, LMX2581, LMX2571, LMX2541
Hello:
I saw in the related question where a user had asked if they could use lower than the -5dBm spec on the RF input power, with the answer being that it tends to work down to about -30dBm, but cannot be guaranteed. So, that pretty much settled my question on RF input power.
But, I have a similar question about the crystal reference input. Here again the LMX2491 data sheet is asking for high drive into low impedance, specifically swing from 0.5 to 2.8V (2.3Vpp) into effectively a 50 ohm load. The data sheet asks for 3V/ns slopes on that input also for best performance. A sine wave at 50MHz at that swing would have a max slope of only 0.722 V/ns. So, the data sheet is effectively asking for that reference output to be squared up, and with effectively a 50 ohm load on the reference input it is also asking for delivered reference power of about +14dBm (with 3dB pad).
But, very few crystal oscillators can provide this. For example, typical handset class VCTCXO's that run about 3V at 2mA for power typically specify that they can drive about 10k. Even the higher power XO's that run 5-10mA typically spend about 4mA on drive output, which into 50 ohms is only about 200mV compared to the 2.3V the data sheet is asking for.
So, I am I correct in assuming that a clock buffer would normally be recommended, even though this is not mentioned in the data sheet? TI happens to have a nice family of these that are relatively low cost and low additive phase noise. An example is the CDCLVC1102, which provides two buffered up outputs from one input. Would this be a part you would recommend for buffering up lower drive crystal references for the LMX2491? Would you advise connecting the two outputs together to get even higher drive capability? Or, could the drive requirement be reduced by using higher impedance padding?
Thanks,
Farron