Part Number: LMX2592
Other Parts Discussed in Thread: LMX2594
This is a continuation of the previous posts which are now closed.
I'm seeing some modulation in the noise at the output of the LMX2592, on a spectrum analyser.
The modulation seems to be fixed between 3.5GHz and 5GHz. The amplitude is not fixed - as I drop the resolution bandwidth, the noise and modulation drops as well. The noise and modulation is visible down to -100dBm.
I measured the above by setting the output frequency to 3GHz and removing the carrier using a notch filter so that I can measure down to -100dBm. Input Reference frequency = 30.72MHz and PFD = 10.72MHz.
Would appreciate if you could have another try to see if you can observe this modulation. The modulation appears like an AM modulation on the noise. The modulation peaks are around 320MHz apart.
Many thanks