This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: How the LVDS Clock of CDCM6208 connect ?

Part Number: CDCM6208


Hi Team,

My customer has a question about CDCM6208. 

Please help me answer the follow question, thank you so much.

I want to connect the LVDS Clock of CDCM6208 to XilinxZynq(XC7Z100-2FFG1156I).

But the VCM-DC of CDCM6208 doesn't satisfy the VICM of Zynq.

Zynq:VICM 0.3-1.425V

CDCM6208:VCM-DC 1.67V(VDD_YX_YY 1.8V)

So I use the the method of AC-couplinng and the DC-bias for specification.

Is there any problems of the clock connection as ug471 Figure 1-72?

Best Regards, 

Tom.Liu