Part Number: LMK04806
Other Parts Discussed in Thread: LMK04616, LMK04832
Hello,
I would like to use the LMK0480x in single PLL mode, see below Fig. 17 from data sheet. Is the OSCin the only possible reference input, or an other input like CLKin1 would be possible? This would imply an hidden mux not visible on the main bloc diagram of §8.2. This connection exist for example in part LMK04616.
I ask this because I want to use an existing board implementing a LMK04806B with this mode, but there are currently no possibility to connect a reference to OSCin. An additionnal mux, external to the LKM04806B would be needed.
Thus I would like check with a TI expert if I have a tiny chance to use this board without modification...
Best regards,