Part Number: SA555
Other Parts Discussed in Thread: LMC555, TLC555
Hello Sir
I am trying to use the pulse-width modulation function of SA555 as an A/D converter.
In the application, I hope SA555 outputs a PWM signal with its duty cycle varying linearly with the voltage amplitude of the external analog signal applied to pin 5 (CONT).
However I got a PWM waveform with variable duty cycle together with variable frequency, and the duty can only vary from 50% to 100% (VCC= 5V or 12V).
I did not apply a continuous pulse train as clock to pin 2. Is it possible to accomplish the function without using a continuous pulse train ?
Best regards
Xiaoming