Part Number: LMK04816BEVAL
Other Parts Discussed in Thread: LMK04816
I have a LMK04816 Eval board from which I am trying to get 125 MHz and 6.25 MHz clock signals. I have a 50 MHz clock signal that I can bring onto the board. The board is equipped with a 122.88 MHz oscillator.
From looking at the TICs Pro software, I do not see a solution where I can generate a 125 MHz clock with a board equipped with a 122.88 MHz oscillator. Given that I am a newbie at this, I would not be surprised if I were missing something.
What documentation would provide me the details I need to achieve my goal? How can I input the 50 MHz signal to use as the reference for the PLL's? (Ideally PLL2) What board modifications do I need to make?
Thanks,
Doug Bailey