Part Number: LMC555
Other Parts Discussed in Thread: SN74LVC1GX04
Hello,
Initially, I was looking to use the LMC555 as an astable vibrator with PNP transitor + integrating capacitor to generate a high frequency (1Mhz) ramp or sawtooth signal, for the purpose of feeding it into a comparator to generate an "analog" PWM with high duty cycle resolution and precise (+consistent) period.
The appealing features of the LMC555 were its high frequency of operation, extremely low power consumption, and self-oscillating capability. However, as I need to tune the frequency precisely to 1 Mhz, the propagation delays and rise/fall times make this unsuitable for my application (I also read in another forum that this would not be appropriate for generating e.g. 2MHz square wave with high precision). As I am not looking to create a 50% duty cycle (rather, a low-power, high resolution ramp/sawtooth signal), I do not think a crystal oscillator would be suitable for my application. Does TI offer any alternatives that I can investigate for my application?
Thanks.