Part Number: LMC555
Hello,
I have a customer wanting to use a LMC555CMM/NOPB in order to have a one-shot timer with length no shorter than 8.13 seconds.
The datasheet specifies the LMC555 timer accuracy at only one set point (5V, 1.1ms set - 1.0ms min and 1.2ms max).
What can the timing accuracy be expected to be at lets say 8.66 second set point?
Thanks,
Reed