Hello,
Is there a range of acceptable duty cycles for the input frequency (priref and secref) to the LMK05318? i.e. from 10% to 90%? Or does it have to be at 50%?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is there a range of acceptable duty cycles for the input frequency (priref and secref) to the LMK05318? i.e. from 10% to 90%? Or does it have to be at 50%?
basedHello,
The duty cycle for the PRIREF and SECREF is not critical as these inputs are edge detect.
Regards,
Liam