This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5110: Any future devices for 1 ms to 10 ms programmable pulse?

Other Parts Discussed in Thread: LMC555

Team,

I have seen from TI.COM that the TPL5xxx family is for a time range of 100ms to 7200s:

http://www.ti.com/clock-and-timing/nanotimers/products.html&sort=p1130;desc

-Do we plan further devices for faster pulse frequency?
The goal would be to have programmable pulse (1 ms to 10ms with a granularity of 0.2ms)  with a power < 1uA and temperature stability < 100ppm/C.
It would be as well a good feature to control the duty cycle (for example 5ms high level and 100 ms low level) but it is not a must.

I have seen as well the LMC555 but the Iq is 50 uA.
-Any other solution available from us that would meet those requirements?

Thanks in advance,

A.