Other Parts Discussed in Thread: LMX2572LP,
Sirs,
The part's integrated phase noise from 12 kHz and 20 MHz is awesome. Well done! In our application we also need great phase noise a 10 Hz offset from carrier, and so we provide a 10MHz OCXO with -145dBc/Hz at 10 Hz offset. My question is, "What is the phase noise figure of merit when locking to an external source? Will it be close to the performance of the LMX2572LP?" (FOM for the LMX2572LP is –232 dBc/Hz and the normalized 1/f Noise is –123.5 dBc/Hz.)
Thanks for your help,
John