Other Parts Discussed in Thread: USB2ANY,
Hello,
I'm working with LMX2571EVM board connected to PC using USB2ANY module. I have st up the port TX (Set of settings F1) to the test frequency 440MHz and it works fine.
I have problems to set up frequency 196.050 MHz on the port RX (Set of settings F2). Some edit boxes e.g. VCO have red background, what does it mean? The VCO=1568.4 MHz that is in the proper range 4.3-5376MHz. I don't see expected tone on the port RX. How could it be fixed? Could you provide settings for Fref = 40 MHz, FoutTX=440MHz and FoutRx=196.05MHz?
Thanks,
Alex