Part Number: CDCVF2505
Other Parts Discussed in Thread: LMK04816, CDCI6214
HI, staff
I'm looking for a feature equivalent device.
ispPAC-CLK5312S (Lattice) is looking for a substitute for EOS.
The requirements are
・ Input frequency: 44 MHz (※ It can be compatible with SSC input CLK)
・Number of output ports: 8-(* No multiplication)
・Skew and jitter performance should be equal to or better than ispPAC-CLK5312S
Please tell me which devices can be recommended by TI.
best regards
cafain