Hi
- In general, in partial assist and close frequency assist modes, if the output frequency range is 1GHz ~ 1.3GHz, and the two frequency switching intervals are 50MHz, what is the frequency lock time?
- If the output frequency range is 1GHz ~ 1.3GHz and the two frequency switching intervals are 50MHz, in the partial assist and close frequency assist modes, how to configure the register and configuration register order?
Thanks