Part Number: LMX2595
Hi ti,
We are using LMX2595 to generate 500-18000 MHz output in steps of 1MHz. We are using 6mA charge pump current with 50KHz loop bandwidth. This is choosen to reduce near by spurious.
With this we are getting less than 200us lock time for all frequency band expect for 11900-12100MHz frequency band.
So for 11900-12100MHz we are thinking of doing fast calibration.
But in page 26 of LMX2595 datasheet there is note stating
"In the range of 11900 MHz to 12100 MHz, VCO assistance cannot be used, and the settings must be: VCO_SEL = 4, VCO_DACISET_STRT = 300, and VCO_CAPCTRL_STRT = 1. Outside this range, in the partial assist for the VCO calibration, the VCO calibration runs. This means that if the settings are incorrect, the VCO still locks with the correct settings. The only consequence is that the calibration time might be a little longer. The closer the calibration settings are to the true final settings, the faster the VCO calibration will be."
What does it mean, we canot do full assist calibration for this band?