Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595
Hello. I need to design 17GHz frequency synthesizer with a bandwidth of 200 MHz and phase noise of -85 dBc @ 1KHz. Initially I thought of generating 8.5GHz and later by using the built in VCO doubler from the LMX2595 IC I can obtain the required objective. For generating 8.5 GHz the feedback divider is to be kept at 21.25 where in the 0.25 fraction is been obtained by changing the numerator and denominator coefficients. But as per our design in the TICS pro software the block N Divider is red coloured which I thought it might result in error and moreover while changing the numerator and denominator coefficients the block N Divider turned to yellow in colour. Even I tried of using large numerator and denominator coefficients but the bug haven't fixed. How to program this register DBLR_IBIAS_CTRL1=3115 in order to make use of VCO doubler and are there any particular set of registers to synchronize phase noise and adjust output power levels. I am new to this TICS pro software. Can anyone help me out to fix this error and meet the above mentioned objective