Part Number: LMX2571
Hi Team,
I have some problem when using the LMX2571 in external vco mode.(TX mode use EXTVCO,RX mode use internal VCO )
1. I can't change the CPOUT voltage from 0.3V~2.7V; I have changed the EXTVCO_CP_IDN/EXTVCO_CP_IUP/EXTVCO_GAIN of Register 42/Register 41.
a)When the EXTVCO_CP_GAIN was set as 1x or 1.5x ,whatever the EXTVCO_CP_IDN/EXTVCO_CP_IUP(2 to 30) is ,the CPOUT always output near 0.08V. EXTVCO_CP_IDN = EXTVCO_CP_IUP
b.When the EXTVCO_CP_GAIN was set as 2x ,whatever the EXTVCO_CP_IDN/EXTVCO_CP_IUP(2 to 30) is ,the CPOUT always output near 2.68V. EXTVCO_CP_IDN = EXTVCO_CP_IUP
c.When the EXTVCO_CP_GAIN was set as 2x ,whatever the EXTVCO_CP_IDN/EXTVCO_CP_IUP(2 to 30) is ,the CPOUT always output near 2.78V. EXTVCO_CP_IDN = EXTVCO_CP_IUP
2.We exchange the RFoutRX port and RFoutTX port in the hardware design.So we set the RFoutRX port to output the TX frequency,but I can't catch the TX frequency in RFoutRX port(pin 16).
I mail my source code to u,the source code have two mode of both internal vco and external vco. In internal vco mode,the LMX2571 can out TX frequency in RFoutRX port(pin 16). But when enable the macro "EXTVCO" ,it can't work fine in external vco mode.
Plz help me check whether the register setting is right?