Part Number: TLC2933A
Hello,
I've got some question about TLC2933A
I want to check wave form of PFD OUT using oscilloscope aside from VCO
The test conditions are as follows
2,7,8,9,11 pin : connect to GND
10 pin : connect to high state
when i apply 3v using power supply at 1,14 pin and 30MHz square wave using function generator at Fin-A,B
how can i set up amplitude and offset to get clear wave form like Figure 2 in datasheet
please let me know if i should change test condition or there is other information to help me
Best regards
Hoseok