This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: LMX2595

Part Number: LMX2595

Hello. As LMX2595 can generate max VCO frequency of about 15GHz and by using the VCO doubler we can attain maximum up to 20GHz. as VCO doubler simply doubles the VCO frequency why don't we obtain 30GHz output frequency if it has maximum VCO frequency is 15GHz.

thanks in advance

  • Hi Singam,

    I noted that you have created 3 posts with the same subject. In future, I suggest you either consolidate all your questions in a single post or use different subject.

    As for your question, the max. output frequency is limited by the process that we are using in this device.