Part Number: CDCE62005
Other Parts Discussed in Thread: CDCM6208
Hi ,
Does CDCE62005 or CDCM6208 support single ended CMOS clock input 50.4Mhz.
Regards,
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can these devices be factory programmed to custom frequencies and provided.
|
Input |
CMOS |
SE |
50.4Mhz |
3.3V |
|
OUTPUTS |
|
|
|
|
|
LVCMOS |
GTX_CLK |
SE |
125mHZ |
/1.8V/2.5V |
|
LVDS |
DIFF_SYS_CLKP/N |
DIFF |
100mHZ |
1.8V |
|
HCSL |
SD_REF_CLKP/N |
DIFF |
100mHZ |
1.8V |
|
LVCMOS |
ETHERNET IC |
SE |
25MHz |
1.8V |
|
HCSL |
FPGA /SERDED |
DIFF |
100mHZ |
1.8V |
|
LVPECL |
CORE CLKP/N |
DIFF |
100Mhz |
1.8V |
|
|
|
|
|
Regards,
Divy
Hello Divy,
The CDCE62005 accepts inputs up to 250 MHz in LVCMOS format.
Please reference table 6.5 in the datasheet.
The CDCE62005 does have internal EEPROM for custom programming during system level testing.
If you are asking about a custom device with pre-programmed EEPROM this is also possibility for higher volume applications.
Regards,