Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594,
Hi,
I have an LMX2594EVM board with Reference Pro interface and am trying to get the best possible phase noise performance from the LMX2594 at 8.2 GHz for a phase noise sensitive application. The LMX2594EVM can be supplied with a source either from a 100 MHz on board oscillator or via the Reference Pro board. I assumed that I would get better performance when using the Reference Pro board however, when I look at the phase noise performance the on-board crystal gives ~10dB better performance beyond ~20kHz, is this correct or have I a configuration problem somewhere? I note that the datasheet says that for best performance the LMX2594 needs a VERY good source for optimum performance.
Many thanks for your help
Best regards
Keith