Dear TI members
I have a question about the device CDCLVC1103. Is there any problem, if I give input to the clock pin (CLKIN) while the VDD pin is not supplied?
If there are any answers please let me know.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI members
I have a question about the device CDCLVC1103. Is there any problem, if I give input to the clock pin (CLKIN) while the VDD pin is not supplied?
If there are any answers please let me know.
Hello Yoshiya,
The datasheet absolute maximum ratings for inputs indicate the input voltage should never exceed VDD + 0.5V. So input should not be supplied to the CLKIN pin until after VDD is supplied.
Regards,