Other Parts Discussed in Thread: LMX2594
Why mechanical vibrations can cause spurious interference within 5 kHz of the signal output by the lmx2572.
We use the LMX2572 as the local oscillator signal of a receiver, but generate an interference signal after adding a fan to the receiver.
We have proven to be mechanical vibration disturbances rather than conducted interference from fans. When the fan draws power from the board through the wire, but does not touch the receiving structure, the output signal of the LMX2572 is such that there is no interference.
Our other local oscillator LMX2594 also has the same problem.
We have proven to be mechanical vibration disturbances rather than conducted interference from fans. When the fan draws power from the board through the wire, but does not touch the receiving structure, the output signal of the LMX2572 is such that there is no interference.