This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: STATUS0 pin Drive

Part Number: CDCM6208

Hi,

Please specify STATUS0 pin (46) IOH\IOL values.

Thanks,

Amir

  • Hi Amir,

    The IOH/IOL values are not characterized. From the datasheet slew rate of 0.5V/ns and the stated capacitance of 10pF, I calculate I = C * dV/dt = 10pF * (0.5V/ns) = 5mA. There is also the VOH/VOL definitions with a test current of 1mA. So it is a reasonable assumption that IOH/IOL cannot exceed more than a few mA before VOH/VOL go out of 80%/20% VDD range.

    Regards,