Part Number: LMK05318
Dear Team,
May I know how to configure GPIO0 as enable?
I didn’t see it on the TCIS Pro GUI.
“Pin 12 GPIO0 for PU, to enable clock gen”
The current code is not set.
please help confirm
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK05318
Dear Team,
May I know how to configure GPIO0 as enable?
I didn’t see it on the TCIS Pro GUI.
“Pin 12 GPIO0 for PU, to enable clock gen”
The current code is not set.
please help confirm
BR
Kevin
Hi Kevin,
The function of GPIO0 is configured at startup. If HW_SW_CTRL input level is LOW or FLOAT, GPIO0 is configured as SYNCN. If HW_SW_CTRL is HIGH, GPIO0 is configured by the ROM page programming. Please see LMK05318 Registers, specifically registers for GPIO_OUT (0x24, R36) and STAT0_SEL/STAT1_SEL (0x30, R48 / 0x31, R49).
I don't see anywhere that GPIO0 can be configured as an enable. Where did the quoted sentence appear?
Regards,