The LMX2595 datasheet indicates that the VCO operates fundamentally from 7.5 – 15.0 GHz, so I did not anticipate seeing any sub-harmonic content at the output (i.e. 0.5*F) when tuning below 15 GHz, but it is there. The 0.5*F level is less than 50 dB down from the tune frequency when tuning above 13 GHz.
I was hoping to use the LMX2595 without a filter at the output given that the VCO operates fundamentally to 15 GHz. The 0.5*F and 1.5*F levels are lower than other PLL ICs that use a doubler to cover the same frequency range, but they would still require filtering.
Is there some internal divide-by-2 being enabled that is causing this or is it just a function of the VCO design?
I did find that setting SEG1_EN (R31[14]) to a ‘1’ dropped the level at 0.5*F by a few dB.
Are there some other register value settings that could be changed to improve the sub-harmonic performance?
Thanks,
John