Other Parts Discussed in Thread: DAC37J82EVM, DAC37J84, LMK04828
Hello,
We were directed to you according to the following message: The part number cannot be recognized; it is this one DAC37J82EVM.
33395 points
Kang Hsia
Hello Valentin,
The DAC37j84 EVMs tested by the data converter group can only be limited by the DAC functions defined in the user software GUI. See below for the few parameters in the GUI.
Unfortunately, the testing capability on the EVM board shop cannot extend to the specific test cases by the customer listed above. However, the LMK04828 is a released part done by the TI clocking group, and the VCO range should be tested on the ATE production test before being placed on the EVM. I recommend the customer to please contact the TI clocking group by posting exact problems that they are seeing when configuring the LMK04828 to the specific cases. They are the experts in the clocking support and will be able to assist much better than us. They can be reached on the E2E forum under clocking.
thanks for your understanding.
Please find our initial query as it was send to the other forum:
'Please find below our query which was originally issued in German language. The translation is done by a person with no technical background.
This question is subject to official claim to your distributor.
Thanks and kind regards
The two internal VCOs of the integrated LMK04828B cannot be operated within the specified frequency range of 2370 - 2630 MHz or 2920 - 3080 MHz. The adjustable frequencies are just within the range or next to it. Therefore, the output frequency can not be set exactly to 160 MHz (divided) but only to about 158.5 MHz. The two tested settings were:
Set VCO0 to 2400 MHz and Divider to 15 to divide to 160 MHz.
Set VCO1 to 3040 MHz and Divider to 19 to divide to 160 MHz.
For two out of three boards, this setting works fine and the PLL2 is locked. PLL1 is correctly locked on all three boards.
The third card is NOK.'
Please let us have a reliable reply how to resolve the problem and do not redirect us again.
Thanks & regards
Magdalena