Hi Team,
I would like to clarify about the PDN pin ESD protection diode that to which power rail it is connected to.
Based on the datasheet page 143 below, there is 200kOhm internal pull up to VDDO_01 for PDN pin.
VDDO_01 could be used as split supply and the voltage could be 3.3V, 2.5V, or 1.8V.
The datasheet states the absolute maximum rating for logic input pins are MAX = "VDD+0.3V".
However, since I was able to see the diode characteristic from PDN pin to VDDO_xx pin using the EVM,
I wanted to clarify whether the ESD diode is connected to this "VDDO_01" or "VDD_DIG (which is always 3.3V)".
Thanks and Best Regards,
Kawai