Part Number: LMX2595
Hello Sir/Ma'am
Will you please suggest one 32 bit microcontroller(specify that ) which support to LMX2595. Fractional divider of that IC is of 32 bit so I need to program that.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2595
Hello Sir/Ma'am
Will you please suggest one 32 bit microcontroller(specify that ) which support to LMX2595. Fractional divider of that IC is of 32 bit so I need to program that.
Hi Pranit,
The register structure of LMX2595 is 24-bit: 1-bit of R/W; 7-bit of Address; 16-bit of Data.
You don't necessary need a 32-bit of 24-bit MCU, you can even use a 8-bit MCU to program the synthesizer.
As you may know, in our EVM kit, we use MSP430 to interface between the synthesizer and the PC. You can get started with this MCU.
If you have any questions regarding the MCU, please make a post to the MCU forum.