Part Number: LMX2595
Respected sir,
Once we obtain the values from the TICS pro software we need to force these values in the registers of the controller. In the practical implementation point of view assuming that i am not using evaluation board I am not able to figure out that whether to load these values in the controller or PLL ic because there are no such controllers available to load these many register values of about 112 registers of 24 bit long. Even though there is no separate dedicated memory space allotted of the register maps such as channel divider and doubler registers, N divider register.
Thanks in advance