Part Number: LMK00804B
Hello,
I need the info regarding the output of LMK00804B, can it drive 50Ohm load? and if yes, what will be the output drive current capability to 50Ohm load?
Regards,
Vinayak
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK00804B
Hello,
I need the info regarding the output of LMK00804B, can it drive 50Ohm load? and if yes, what will be the output drive current capability to 50Ohm load?
Regards,
Vinayak
Hi Vinayak,
LMK00804B is designed to drive LVCMOS / LVTTL loads. A 50-ohm load is a heavy load for the driver, I would consider using a high impedance load.
I don't anticipate an issue with 50-ohm load to GND. The VOH values in table 7.7 were obtained with a 50-ohm load to VDDO/2.
Kind regards,
Lane