hello. i have a question i have two diferential lvds clock from two separate hdmi source and i want to synchronize the two diferential clock.
I would like to use LMK00334, maybe or if you can recommend a new one. THX
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello. i have a question i have two diferential lvds clock from two separate hdmi source and i want to synchronize the two diferential clock.
I would like to use LMK00334, maybe or if you can recommend a new one. THX
Hello,
For synchronizing two frequencies, one option would be to use one HDMI input as a reference source to a PLL and have the other derived from the first. These would then be aligned with some propagation delay.
Could you be more specific about what frequencies you are looking to support?
Regards,
Liam
Hello I want to synchronize from three sources of hdmi the pixel clock(clok+,clock-), so one of the sources will be the reference and the other two sources will be synchronized with the reference, the maximum frequency will be 133Mhz
.
Theoretically I think if I could synchronize the pixel clock I could make a fast switch.
I use tmds442 hdmi switch with 3 inputs and two outputs, my customer want fast switching.
If you could give me an idea which circuit to use I would really appreciate it thx.
Hi Varga,
If you can use one as reference and get the others from the reference, then there's a long list of TI clock gens to select from, depending on performance requirements. Please refer to the selection guide: http://www.ti.com/clock-and-timing/generators/products.html
Regards,
Hao