This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVD1204: how to design with 3.3V LVCmos INPUT? Do we have some recommend circuit for 3.3v Lvcmos input?

Part Number: CDCLVD1204


Hi team,

how to design with 3.3V LVCmos INPUT? Do we have some recommend circuit for 3.3v Lvcmos input? Thanks.

  • I would not recommend a 3.3V LVCMOS input as the input voltage could exceed the recommended operating maximum. Consider using a level shifter or clock buffer to translate the levels.

    A simpler alternative would be to create a voltage divider using large resistors to attenuate the signal level, however this is not recommended in many cases as it can have a negative impact on signal integrity. You could simulate the signal integrity using the IBIS model.

    Kind regards,
    Lane