Part Number: PLLATINUMSIM-SW
Other Parts Discussed in Thread: LMX2492
Dear all,
I am facing some problems with PLLatinumSIM (v.1.5.3.0) when trying to get a precise Lock Time using the Discrete LT Function. The process that prompts me to the error messages is the following:
- Upon opening the software, I choose LMX2492 as the PLL model.
- I choose Feature Level = Advanced
- I go straight to Lock Time tab and check "Show discrete model" and then press on "Calculate Discrete LT". I leave all the default values unchanged.
- I get an unhandled exception error window with the debugging info shown at the bottom of this message
Apart from this problem, I am also having trouble loading OSC Phase Noise metrics into the program. The thing is that I am trying to model some OSC that is not a Crystal oscillator and, as such, when I input the Phase noise metrics in the program, I get a yellow box indicating that the values violate the 3 point model assumption. I tried loading a Phase Noise data .txt file and the software shows "Data Loaded" but the OSC phase noise does not show correctly in the Phase Noise graph. The Phase Noise data that I am trying to load into the program is as follows:
1000,-98.00
4000,-98.00
6000,-95.00
10000,-105.00
40000,-120.00
100000,-120.00
1000000,-130.00
10000000,-135.00
The debugging info for the Lock Time calculation Unhandled Exception:
| Consulte el final de este mensaje para obtener más detalles sobre cómo invocar a la depuración Just-In-Time (JIT) en lugar de a este cuadro de diálogo. ************** Texto de la excepción ************** System.NullReferenceException: Variable de objeto o de bloque With no establecida. en Microsoft.VisualBasic.CompilerServices.Symbols.Container..ctor(Object Instance) en Microsoft.VisualBasic.CompilerServices.NewLateBinding.LateGet(Object Instance, Type Type, String MemberName, Object[] Arguments, String[] ArgumentNames, Type[] TypeArguments, Boolean[] CopyBack) en TIPLLatinumSim.CalculateLockTime.GraphLockTime_Discrete(TIPLLatinumForm& frm, LockTimeParameters& ltparameters, LoopFilter& filter, Object& LockTimeSheet) en TIPLLatinumSim.TIPLLatinumForm.CalculateLockTime(Object Locktimesheet) en TIPLLatinumSim.TIPLLatinumForm.CalculateDiscreteLTButton_Click(Object sender, EventArgs e) en System.Windows.Forms.Control.OnClick(EventArgs e) en System.Windows.Forms.Button.OnClick(EventArgs e) en System.Windows.Forms.Button.OnMouseUp(MouseEventArgs mevent) en System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks) en System.Windows.Forms.Control.WndProc(Message& m) en System.Windows.Forms.ButtonBase.WndProc(Message& m) en System.Windows.Forms.Button.WndProc(Message& m) en System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m) en System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m) en System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam) ************** Ensamblados cargados ************** mscorlib Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3416.0 built by: NET472REL1LAST_B Código base: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll ---------------------------------------- TIPLLatinumSim Versión del ensamblado: 1.5.3.0 Versión Win32: 1.5.3.0 Código base: file:///C:/Program%20Files%20(x86)/Texas%20Instruments/PLLatinumSim/TIPLLatinumSim.exe ---------------------------------------- Microsoft.VisualBasic Versión del ensamblado: 10.0.0.0 Versión Win32: 14.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/Microsoft.VisualBasic/v4.0_10.0.0.0__b03f5f7f11d50a3a/Microsoft.VisualBasic.dll ---------------------------------------- System Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3416.0 built by: NET472REL1LAST_B Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll ---------------------------------------- System.Core Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3429.0 built by: NET472REL1LAST_C Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll ---------------------------------------- System.Windows.Forms Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3324.0 built by: NET472REL1LAST_C Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll ---------------------------------------- System.Drawing Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll ---------------------------------------- System.Configuration Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll ---------------------------------------- System.Xml Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll ---------------------------------------- System.Runtime.Remoting Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Runtime.Remoting/v4.0_4.0.0.0__b77a5c561934e089/System.Runtime.Remoting.dll ---------------------------------------- System.Windows.Forms.DataVisualization Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.DataVisualization/v4.0_4.0.0.0__31bf3856ad364e35/System.Windows.Forms.DataVisualization.dll ---------------------------------------- System.Windows.Forms.DataVisualization.resources Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.DataVisualization.resources/v4.0_4.0.0.0_es_31bf3856ad364e35/System.Windows.Forms.DataVisualization.resources.dll ---------------------------------------- System.Data Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3260.0 built by: NET472REL1LAST_C Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_32/System.Data/v4.0_4.0.0.0__b77a5c561934e089/System.Data.dll ---------------------------------------- Accessibility Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll ---------------------------------------- Microsoft.VisualBasic.resources Versión del ensamblado: 10.0.0.0 Versión Win32: 14.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/Microsoft.VisualBasic.resources/v4.0_10.0.0.0_es_b03f5f7f11d50a3a/Microsoft.VisualBasic.resources.dll ---------------------------------------- System.Windows.Forms.resources Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.resources/v4.0_4.0.0.0_es_b77a5c561934e089/System.Windows.Forms.resources.dll ---------------------------------------- mscorlib.resources Versión del ensamblado: 4.0.0.0 Versión Win32: 4.7.3056.0 built by: NET472REL1 Código base: file:///C:/WINDOWS/Microsoft.Net/assembly/GAC_MSIL/mscorlib.resources/v4.0_4.0.0.0_es_b77a5c561934e089/mscorlib.resources.dll ---------------------------------------- ************** Depuración JIT ************** Para habilitar la depuración Just In Time (JIT), el archivo de configuración de esta aplicación o equipo (machine.config) debe tener el valor jitDebugging establecido en la sección system.windows.forms. La aplicación también se debe compilar con la depuración habilitada Por ejemplo: <configuration> <system.windows.forms jitDebugging="true" /> </configuration> Cuando esté habilitada la depuración JIT, cualquier excepción no controlada se enviará al depurador JIT registrado en el equipo en lugar de controlarlo mediante el cuadro de diálogo. |
Some of the info is shown in spanish as it is my system's language.