This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62002 Pin Connection - Ref -, Pin 30

Hi,

For the PCB i have designed and had fabricated, connected Pin 30 (Ref -) to high logic level through a 10kohm resistor - this was in error.

The datasheet states that this pin must be pulled down.

I have connected a crystal oscillator to Pin 29.

I can see the inverted logic symbol on the pin in figure 22.

Hence, with Pin 30 pin connected to a high logic level, does this stop the Ref + Pin 29 functioning as an input ?.

Thanks and regards,

Richard.