Hi,
I have implemented the CDCE62002 in a design that uses two references - one crystal oscillator as the CMOS input, and another crystal using the CDC62002 oscillator circuitry.
The two frequencies are do not share any common factors, hence the use of two crystals.
Hence i am using the CDCE62002 to provide clocks based on either input.
The performance of the CDCE62002 is a sub Picosecond jitter.
Since i wish to use two distinct frequencies with low jitter clocks, is there an alternative way of providing the two frequencies from simple crystal oscillators that exhibit the same low jitter ?.
I could employ logical switching to distribute the clock to the relevant IC.
I ask this as i cannot find any literature for clock generation that does not employ phase locked loops (PLL).
Are there any circuits that use crystals, and from memory, such as a simple inverter, that produces sub-picosecond clock jitter ?. is only a single freuqency is required and that frequency is available as a crystal ?
Can sub-picosecond clock jitter only be provided by CDCE62002 family IC's ?
Arte there clock multipliers that provide the same low jitter (sub-picosecond) that can be used ?
Thanks in advance for any guidance,
Regards,
Richard.