Part Number: LMK03328EVM
Other Parts Discussed in Thread: USB2ANY, , LMK03328
I am trying to communicate via I2C using a USB2ANY (HPA665-001) with a LMK03328EVM (SV601123A-002) with no success. In TICS Pro --> USB Communications, the USB2ANY is recognized: USB Connected indicator is green, Select USB2ANY = 887F1B5125001C00, Bit Rate (kbps) = 400. When I click Identify, the LED on the USB2ANY flashes. I2C address of the EVM is 54 when I verified as GPIO1 = 0V (MID jumpered to LOW). When I click on "Scan I2C Bus" I get "No device found". I've tried varying the bit rate to no success. I'm not why I can't just plug the USB2ANY into J28 (which I populated) on the LMK03328 EVM and have the TCIS Pro GUI recognize the LMK03328 component.