Part Number: LMK04208
Other Parts Discussed in Thread: LMK04828, , LMX2594, LMK04832
Hello,
I need to design a clock tree to support the Xilinx RFSoC, and I have a few questions about Clock distribution devices supporting JESD204B.
- What makes a device to be JESD204B compliant?
If I understood correctly, it suppose to generate both the high speed (clean) clock to be the sampling clock of a data converter,
and the SYSREF clock, which is a lower frequency but with the same phase (Sampling clock divided by certain factor) + capabele of phase alignment to compensate PCB traces.
- Why the LMK04208 has not been declared as JESD204B compliant? (how it differs from LMK04828 for instance?)
- If I use a non JESD204B compliant device to generate both the SYSREF, and a Reference clock for other (high frequency) PLL which generates the Sampling clock, will I comply the JESD204B?
I saw a design (Xilinx RFSoC Eval board - ZCU111, https://www.xilinx.com/products/boards-and-kits/zcu111.html)
which uses the LMK04208 to generate the SYSREF Clocks for the RFSoC, and the Ref.+Sync. Clocks for the LMX2594 to be the Sampling clocks.
- When do I need to assert the SYNC input to a device, to ensure that the output phase of all clocks is the same?
In the same example (Xilinx RFSoC Eval board - ZCU111), The SYNC to the LMX2594 is not asserted.
- The High frequency Sampling clock for the data converter must be clean, to not degrade the performance (SNR etc.). Does the SYSREF also influence the performane and must be clean as well?