This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK62A2-100M: Pullup in the OE PIN not present

Part Number: LMK62A2-100M

Dear all, I used yours LMK62A2-100M on a data acquisition board I designed.

In my design I connected the GND (PIN 3) , the +3.3V (PIN 6)  and the +-LVDS Output (PIN 4 & 5). I did not connect (I left it NC) the OE input (PIN 1) because in your data sheet (on page 3, PIN description) there was written that the pullup to 3.3V was internal. It seem that this is not the case...

If I pullup the OE PIN than everything start working otherwise the oscillator is high impedance. Is there a mistake in the data sheet or did I make something wrong?

Best regards

Andrea Puccini