Tool/software: WEBENCH® Design Tools
Hi,
We have a LMX2594 EVM and we are learning how to use it.
First, we found when we set the output frequency to 100-500 MHz, the output waveform is near a square wave. Is there any reason why it is not sinusoid?
In addition, we want to use LMX2594 to generate a frequency ramp. What's is the minimum starting frequency in the "Automatic Ramping" mode? For example, if we want to start from 1GHz and go to 2GHz, and then come back to 1 GHz and repeat this process continuously, is it possible? Or is it possible to have any sample code to do it?
What's more, in the "Manual Ramping" mode, we set the "Step Frequency (MHz)" to 1000 MHz and pressed "Clock Ramp" button. However, the final frequency we obtained is much less than 500MHz (about 100 MHz). Is there any reason why this? Our starting frequency is 1000 MHz.
Thanks a lot.