This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: Output resolution

Part Number: LMX2592

For a desired output frequency between 99-111MHz, what's the best-case resolution I can achieve with LMX2592?

Can I achieve a resolution of 25kHz with LMX2592?

  • Hi Gregory,

    Assume there is no output divider and VCO pre-scalar, the resolution of a fractional-N PLL is equal to fpd/DEN. 

    In your case, given CHDIV=36, Pre-scalar = 2 and resolution = 25kHz at the output.

    resolution x CHDIV = fpd x pre-scalar / DEN.

    If you set fpd = 72MHz, then DEN=160. Changing NUM by 1 will change the output freq by 25kHz.